Reset SQL Credentials
Procedure
-
You must define your configuration in the
silentinstaller.yml file. Update the following
parameter in the silentinstaller.yml file:
Parameter Description WEBCLIENT_INSTALLATION_PATH: "" Enter the Web Client Installation path in which you want to install. For example, WEBCLIENT_INSTALLATION_PATH: "/home/ administrator/install/" PLANT_APPS_DB_SERVER: "" Enter the Plant Applications database server hostname that you want to connect with the Plant Applications Web Client. PLANT_APPS_DB_INSTANCE: "" Enter the name of the instance of the SQL server. You can leave this parameter empty if not using an instance. For example, PLANT_APPS_DB_INSTANCE:"sa"
Note:Do not add a backslash (\) when entering the instance name.PLANT_APPS_DB_NAME: "" Enter the Plant Applications Database name. For example, PLANT_APPS_DB_NAME:"SOADB"
PLANT_APPS_DB_USERNAME: "" Enter the username that has permissions to access the database you entered. PLANT_APPS_DB_PASSWORD: "" Enter the password for the username you entered. PLANT_APPS_DB_PORT: "" Enter the SQL Server port. - Access the utility.sh file in the plantapps-enterprise-webclient-<buildno> folder.
-
Provide execution permissions to utility.sh file by
running the following command:
sudo chmod +x your/pathto/installer/plantapps-enterprise-webclient-<buildno>/utility.sh
-
Run the utility.sh file by running one of the following
commands:
- If you are running this utility directly on the Enterprise Edition Web Client node:
<installer path>/plantapps-enterprise-webclient-<buildno>/sudo ./utility.sh -l -sql reset
- If you are running this utility remotely on the Enterprise Edition Web Client node:
<installer path>/plantapps-enterprise-webclient-<buildno>/sudo ./utility.sh -r -sql reset
Docker secrets are created based on the values you entered, and the Docker stacks are redeployed so that the containers use the new credentials. - If you are running this utility directly on the Enterprise Edition Web Client node: