Configure Plant Model
About this task
Procedure
- Access Plant Applications Administrator.
- Create a department named Receiving and Inspection.
- Create a production line named Received Material Lots in the department. This is the default name. If you want to change it, you must also change the property name in Property Definition (in the ERP App category, MaterialLot Import group).
-
Create a production unit named Receiver in the production line to handle
Receiving Inspection tasks, and configure an inactive production event model for
the Receiver sub-type on this production unit.
- Create a production unit named Received Material Lots-<UOM> in the production line for every UOM used by materials that you want to inspect.
- Create an inactive production event model for the correct Received Material Lot-<UOM> event sub-type on these production units.
-
Create an inactive user-defined event model using the Inspection Sample event
sub-type on these production units.
- Ensure that the inspected materials for a given UOM are associated with the Received Material Lots production unit configured for the same UOM. You can specify the unit using Plant Applications Administrator or import a material master import document (MMID) during ERP integration.
- For the organization codes that you want to use with external systems (such as an ERP application), add the values in the Extended Information field in the Edit <production unit name> window.
- In the Production Statuses section, ensure that the check boxes for the statuses related to Receiving Inspection are selected. In addition, set the Unassigned status as the default one.
-
Set the valid transitions for Receiver unit as described in the following
table.
Status Valid Transitions Pending Unapproved Supplier - Open
- Unapproved Supplier
Unapproved Supplier Open Open Defined Defined - Waiting Inspection
- Periodic Inspection
Periodic Inspection Waiting Inspection Waiting Inspection - Inspection in Progress
- Pending MRB/NCR
- Receiver Complete
Inspection in Progress - Receiver Complete
- Pending MRB/NCR
Pending MRB/NCR - Receiver Complete
- Risk Release
Receiver Complete None Risk Release Pending MRB/NCR -
Set the valid transitions for units where the lots are created as described in
the following table.
Status Valid Transitions Unassigned Open Open - Accept
- MRB/NCR
- Periodic Inspection
Accept - DIT
- Open
- Risk Release
- RTV
- Scrap
MRB/NCR - Accept
- DIT
- Open
- Periodic Inspection
- Risk Release
- RTV
- Scrap
Periodic Inspection None DIT None Risk Release - DIT
- RTV
- Scrap
RTV None Scrap Accept - Create a variable group for the Receiver production unit called “Calculations”.
-
In this variable group, create a variable named Material ID with the following
specifications:
- Data source: Autolog
- Event type: Production Event
- Subtype: Receiver
- Data type: Integer
- Create a variable group for each Received Material Lots (<UOM>) production unit called “Sampling Engine”.
-
In this variable group, create a variable named AutoGeneratedSample with the
following specifications:
- Data source: Autolog
- Event type: User-Defined Event
- Subtype: Inspection Sample
- Data type: Logical
Note:In order to generate samples, set the parameter ClearAppliedProductIfSame (found in Administer Site Parameters) to False.