Configure Global and Product Settings
Procedure
- Access Plant Applications Administrator.
- Create a production event sub-type named Receiver. This event must have UOM defined as "Lot" which is available from the list.
-
Create a user-defined event sub-type named Inspection Sample. Select the
Require Selection Of Event Duration check box when you so do.
Note:The name of the event sub-type is case-sensitive and must be Inspection Sample only.
-
Create an engineering unit record for every unit of measurement (UOM)
associated with the material lots that you want to inspect.
-
Create a new production event sub-type named Received Material Lot-<UOM> for
every UOM that you have created. Configure these new event sub-types to use the
appropriate UOM. Ensure that the name of the receiver UOM matches the UOM
selected from the list. If the UOM is not listed, follow Step 4 to add it.
-
Create a product family named Receiving and Inspection.
Note:If there are no products in the system, create at least one serialized and one non-serialized product.
-
Create a product property named Receiving and Inspection, and configure it to
create the characteristics on the Receiving and Inspection product family.
-
Create a characteristic for every material that you want to inspect using the
Receiving Inspection product property.
-
Make sure that every inspected material under the Receiving and Inspection
family has the default characteristic for the Receiving Inspection product
property set to a characteristic that matches the product code.
-
Create the following specification variables under the Receiving and Inspection
product property:
Specification Data Type Description Auto Complete Logical If set to true, the sampling engine will not create any tests, and you can access Inspection Results to complete material lots. TCR-Critical Criteria String The name of the variable group the sampling engine will use to generate tests marked as critical. TCR-Part-specific Criteria String The name of the variable group the sampling engine will use to generate tests marked as part-specific. TCR-Common Criteria String The name of the variable group the sampling engine will use to generate tests marked as common. %Samples to test (for Non-Serialized products) Float The percentage of lot quantity to be tested. For example, if the value is 10%, and the received material lot has 50 lots, then five samples will be generated. %Serial Numbers to test (For Serialized products) Float The percentage of lot quantity to be tested. - Enter the target specifications for all characteristics for the specification variables that you have created.