STATUS | The status of the route. |
NAME | The name of the route. |
MATERIAL | The material number used in the route. |
MATERIAL DESC | The description of the material. |
PRODUCTION LINE | The name of the production to which the route belongs. |
DESCRIPTION | The description of the route. |
LAST MODIFIED | The date and time when the route was last modified. The date and time appear in the format mm/dd hh:mm (for example, 03/27 10:58). |
MODIFIED BY | The name of the user who has modified the route the last time. |
REVISION | The number of times the route has been revised. |
ROUTE
LOCK/UNLOCK |
The status indicating whether the route can
be changed or not. The ROUTE
LOCK/UNLOCK toggle button by default
is unlocked. When the route is in the
UNLOCKED status, then all
the tabs on the Edit Route
page are disabled and the user cannot make any
changes. |