Creating a Minor Revision
Procedure
-
In the Route Editor page, perform one of the following tasks:
- If you want to create a revision of a released route, select Released.
- If you want to create a revision of an archived route, select Archived.
-
Select the route whose revision you want to create.
The View Route page appears.
-
Select
, and then select Create Minor Revision.
The Revise Route window appears, displaying the route details.Note:- The name, description, production line, material, and BOM formulation are copied from the latest version of the route and cannot be modified.
- The REVISION box is disabled and populated with the
next incremental number.
For example: If the existing Route revision number is 0.0, then the revision number will be incremented to 0.1 during a minor revision. The revision number is incremented in decimal steps.
-
Select Next.
The Edit Route page appears. The operations, resources, BOM items, properties, and documents linked to the route are the same as that of the latest version of the route.Note:
- You cannot add, copy, or delete operations in the route. But you can select additional equipment or deselect the equipment for the operations.
- You cannot modify operations behaviors. But you can select or deselect labor types.
- You can setup labor types, machine labor codes, and people labor codes for an equipment.
- You can assign or delete property group(s) by definition and update property default values.
- You cannot attach document(s) and/or URLs, or upload document(s). Add
and upload
buttons are disabled. However, you can revise the documents with minor revision type.
- You cannot add or modify the tools.
-
Select Save.
The route revision is created and is in the draft state. The value in the REVISION box is revised to the next decimal number.