Access the Equipment Summary
The OEE Dashboard application in Plant Applications enables you to access the summary of Equipment for the Production Lines in a Department or Production Site or Production Units in a Production Line. The Equipment summary appears as a series of Donut charts for KPIs such as OEE, Performance, Quality, and Availability.
Procedure
- Log in to the Plant Applications Web Client.
- Select
.
A page displaying the Equipment summary appears. - Select an option in the View by box as described in the following table.
Option Description Summary When you select this option, a summary for all the Production Lines with Low OEE across departments appears in the page. This option is selected by default. Lines When you select this option, an In box appears, in which you can select a Department. After you select a Department, the page displays the Equipment summary for the Production Lines within the selected Department. Units When you select this option, an In box appears, in which you can select a Production Line. After you select a Production Line, the page displays the Equipment summary for the Production Units within the selected Production Line. - In the drop-down list box next to the View by box, select a time range as described in the following table.
Option Description Current Shift Select to access the summary of the Equipment in the ongoing shift. By default, this option is selected. Last Shift Select to access the summary of the Equipment in the shift prior to the current shift. Today Select to access the summary of the Equipment on the current Production Day. Yesterday Select to access the summary of the Equipment from the day prior to the current Production Day. Current Week Select to access the summary of the Equipment within the ongoing Production Week. Last Week Select to access the summary of the Equipment within the Production Week prior to the current Production Week. Custom Select to access the summary of the Equipment within a date and time range that you specify by using a calendar window. The following calendar window appears when you select the Custom option.
To specify a custom date and time range in the calendar window:- In the START DATETIME section, select a date and enter a time in the format hh:mm:ss.
- In the END DATETIME section, select a date and enter a time in the format hh:mm:ss.
- Select Apply.
Note:If there are no shifts configured for the plant, the Current Shift and Last Shift options do not appear.The time range calculations for the Current Shift and Last Shift time range options are based on the
Site_Parameters
table rather than theCrew_Schedule
table.In the page displaying the Equipment summary:- The time range that you select appears.
- The Donut charts summarizing OEE, Quality, Performance, and Availability for each KPI appear
Note:Each KPI card displays the following status information.These KPI metrics are based on the OEE Aggregation Store setting. If OEE Aggregation Store is set to False, the values are calculated on the fly every time the chart is opened or refreshed. If it is set to True, the values are populated from the OEE Aggregation tables. For more information, refer to the About OEE Aggregation Store topic.Status Colors Range Good Blue > 85 percent Moderate Yellow > 50 percent and <= 85 percent Low Red <= 50 percent Note:The maximum value for the KPIs are set to 100% by default. However, you can override this by setting OEE Max Limit Override to true. The OEE Max Limit Override flag allows the OEE cap beyond 100%. When this flag is set to false and the KPI actual value is more than 100%, the value is defaulted to 100% in the chart. - To access the detailed KPI information, select
in the KPI card. The Availability KPI card with the detailed KPI information also includes summary statistics.
Note:The detailed KPI information is not available for the OEE KPI card.The Pareto and Waterfall charts that show the detailed information for the selected KPI appear in the page displaying the Equipment summary. When you select + for a KPI card, the charts appear, displaying information about the KPI as described in the following table.KPIs Description Quality Displays the following details about the calculated Quality by product: - Scrap Breakdown: A Pareto chart displaying the top five reasons for the scrap breakdown. Select Get By Duration to access the breakdown information by duration.
- Loss By Product: A Waterfall chart displaying losses by product.
Note:In the View by box for a chart, select Quantity or Count to access the data according to the selected option in the chart.Performance Displays the following details about the calculated Performance by product: - Speed Loss Breakdown: A Pareto chart displaying the top five reasons for the speed loss breakdown.
- Speed Loss By Category: A Waterfall chart displaying speed losses by category.
Note:In the View by box for a chart, select Duration or Count to access the data according to the selected option in the chart.Availability Displays the following details about the calculated Availability related to the uptime of the machine: - Summary Statistics: A list of the number of events, total downtime, mean time to repair (MTTR), and mean time between failures (MTBF) values. By knowing MTBF and MTTR values, you can schedule around the availability of the Equipment while informed of the time between failures and the time it takes to resolve issues, thus enhancing OEE.
- Downtime Breakdown: A Pareto chart displaying the top five reasons for the downtime breakdown.
- Downtime by Category: A Waterfall chart displaying downtime by category.
- A list of reasons for the downtime and color-coded charts that display uptime and downtime for the selected time range.
Note:In the View by box for a chart, select Duration or Count to access the data according to the selected option in the chart.When you hover over any bars in the charts, the tooltip displays the information about the attributes described in the following table.Attribute Description Fraction Corresponding percentage of the total downtime Count Number of events Duration Downtime duration - Optional: Select
, then select the NPT check box, and then select Apply to include any non-productive time (NPT) in the results. For more information, refer to the About Non-Productive Time in Downtime Calculations topic.