L to R: Hudson Gilmer, Co-Founder and CEO, LineVision, Sal Gill, Global Product Line Leader Transmission Grid Automation, GE, Alex Houghtaling, VP Sales, LineVision, Massimo Nardi, Director of Sales, North Region, GE and Jonathan Marmillo, Co-founder, VP Product, LineVision
L to R: Hudson Gilmer, Co-Founder and CEO, LineVision, Sal Gill, Global Product Line Leader Transmission Grid Automation, GE, Alex Houghtaling, VP Sales, LineVision, Massimo Nardi, Director of Sales, North Region, GE and Jonathan Marmillo, Co-founder, VP Product, LineVision
BOSTON, Dec. 7, 2022 /PRNewswire/ - GE Grid Solutions (NYSE: GE), bringing together advanced grid technologies and expertise to help electrify our world and accelerate the energy transition, and LineVision, the global leader in Dynamic Line Ratings (DLR), have formed a partnership to deliver the world's first integrated suite of Grid Enhancing Technologies (GETs), providing utilities with an end-to-end Dynamic System Rating (DSR). GE and LineVision will combine Dynamic Line Ratings (DLR), Dynamic Power Rating (DPR), and Optimal Power Flow Controllers (OPFC) to significantly increase transmission capacity while ensuring grid reliability.
Globally, the need to optimize the existing transmission grid and expand its ability to carry more clean energy has never been more urgent. In the US, the National Renewable Energy Laboratory has reported that grid capacity must triple to achieve zero carbon by 2035[1]. A lack of sufficient capacity is preventing 1.4 terawatts of renewables and energy storage from connecting to the grid and this year has caused nearly $100 billion in congestion costs that are paid by consumers[2],[3].
Europe aims to reduce greenhouse gas emissions by at least 55% by the end of the decade compared to 1990 levels and source 40% of its energy consumption from renewable energy[4]. However, this shift to renewable energy sources won't be realized without expanding transmission capacity which is already lacking, resulting in congestion and record-high prices of electricity.
Australia is preparing for the clean energy transition with 67GW of renewable energy projects in the interconnection queue but grid congestion has prevented much of that capacity from becoming operational[5].
"Our utility clients know that increased renewable integration and electrification requires a flexible and dynamic grid," said Claudia Cosoreanu, CTO of GE Grid Automation, Grid Solutions. "Dynamic System Rating will change how utility operators optimize the grid and enable them to integrate more renewables using the same infrastructure. This will reduce the amount of investment needed to reach decarbonization goals and keep the electricity costs to affordable levels for everyone."
"These technologies represent a new model of grid infrastructure investment which will accelerate the transition to a net zero grid," said Hudson Gilmer, CEO of LineVision. "Transmission capacity is the limiting factor preventing the clean energy economy from becoming a reality. The solution now exists to rapidly and fully optimize our existing assets."
###
(1) National Renewable Energy Laboratory. 100% Clean Electricity by 2035.
(2)Lawrence Berkley National Lab. Queued Up.
(3)Bloomberg. Negative Power Prices? Blame the US Grid for Stranding Renewable Energy.
(4)European Commission's 2030 Climate Target plan.
(5)PV Magazine: "WoodMac: Grid congestion chokes renewables investments in Australia"
GE Vernova to deliver two SF₆-free 420 kV gas-in...
GE Vernova has been selected by Sterlite Grid 32 L...
GE Vernova and Drydocks World awarded Ostwind 4, t...