Valley city at night under moonlight, symbolizing reliable energy through GE Vernova grid solutions

Press Releases

GE Vernova’s STATCOM system to improve grid stability in Germany

September 1, 2022

Paris, FRANCE — September 1, 2022 — GE Vernova Renewable Energy's Grid Solutions business (NYSE: GEV) has entered into a framework agreement to deliver Static Synchronous Compensators (STATCOMs) in the coming years to Germany's transmission system operator (TSO) 50Hertz. As a part of the framework agreement, GE Vernova has been chosen to deliver the first Static Synchronous Compensators (STATCOMs) to increase grid stability.

Each STATCOM systems will supply ±300 Mvar at Elia Group's 50Hertz Transmission GmbH (50Hertz) substation in Bad Lauchstädt. The substation in the heart of the 50Hertz grid area plays an important role for the transmission of growing amounts of electricity from renewable sources. It is – for example – the starting point of the so-called 380 kV Südwestkuppelleitung from the region of Lower-Saxony via Thuringia to Bavaria.

As electrical transmission grid operators face increasing demand and complexity with an influx of renewable energy sources, GE Vernova's patented STATCOM technology offers an efficient, dynamic solution. The custom-designed system provides grid operators with reactive power compensation and improved range of operational voltage, resulting in a faster response time and with a smaller footprint than traditional static VAR compensator (SVC) solutions.

“50Hertz's strategy is to enable 100 percent renewables in electricity consumption in our grid area by 2032 and to help industrial companies to decarbonize their procedures," said Dr. Frank Golletz, Chief Technical Officer of 50Hertz. "Large coal-fired power plants, and therefore powerful generators, will exit the electricity system and in order to maintain the required voltage we will need to invest massively in dynamic as well as static reactive power compensation equipment," Golletz states. “The award of the contract to GE Vernova is an important building block in this strategy,” he added.

“Highly reliable and easy to integrate into both existing and new infrastructures, GE Vernova’s STATCOM system also has given 50Hertz an economical solution,” said Johan Bindele, GE Vernova’s Grid Solutions’ Grid Integration Leader. “As grid networks change with the introduction of renewable power sources, utility and transmission network operators are increasingly recognizing that GE Vernova’s grid solutions are necessary—providing dynamic voltage support while maintaining the reliability and efficiency of the power supply.”

For this project, the latest generation STATCOM solution is a Voltage Source Converter (VSC) technology based on MMC architecture1  leveraged from GE Vernova’s robust power electronics experience. This design provides more stable output power generation than other competitive solutions, helping customer grids handle faults and fault recovery within the industry’s best performance. This more powerful design, combined with GE Vernova’s experience from more than 400 shunt connected FACTS solutions, offers customers a complete, world-class, digitally enabled solution. 

GE Vernova’s Alternating Current Solutions (ACS) teams based in Berlin and Dresden, Germany, will deliver the turnkey supply of the two hybrid STATCOMs, given their vast experience in delivering turnkey projects for 50Hertz Transmission GmbH. The project will cover engineering, integration, supply, construction including Civil Works, installation, mechanical completion, testing, commissioning and thereafter maintenance services for a period of five years. It will be executed with our German Civil Works partner RBS Raffinerie Bau Schwedt GmbH.  Completion is planned for 2025 and 2027.

                                                                                           ###

(1) The Modular Multilevel Converter (MMC) is a scalable technology, built up by identical but individually controllable submodules that make high voltage and power capability possible.