Located in the French Alps on the Eau d’Olle river near Vaujany, Isère, France, the Grand Maison Hydropower Plant is the largest pumped‑storage facility in France with an installed capacity of 1,800 MW. Commissioned in the 1980s as part of France’s strategic renewable energy infrastructure, it uses a high hydraulic head of around 920–955 m to deliver large‑scale energy generation and storage for the national grid.
During the initial construction, GE Vernova supplied the plant’s four 157 MW Pelton turbine-generating units to harness the site’s high-head potential and maximize efficiency. Around 35 years later, GE Vernova supplied four new Pelton turbines as part of the refurbishment project, with significant improvements to the runners and injectors. These upgrades increased output by more than 8%, raising the unit capacity to 170 MW. In addition to the Pelton turbines, the facility includes eight GE Vernova reversible pump-turbine units, enabling it to function as a pumped-storage system that stores energy during periods of low demand and generates electricity during peak demand.
The Grand Maison Hydropower Plant remains a cornerstone of France's energy flexibility, offering around 1,400 GWh of renewable, low-carbon energy annually while supporting grid integration of variable renewable sources like wind and solar.