Located in the municipality of Finhaut in Valais, Switzerland, the Nant de Drance
pumped-storage hydropower plant is a major energy storage asset with an installed
capacity of 900 MW. The plant is located 600 meters underground between the Vieux Emosson upper reservoir and the Emosson lower reservoir. Designed to provide flexibility to the Swiss and European power systems, it plays a key role in grid stability, security of supply and the integration of intermittent renewable energy.
GE Vernova supplied the project’s electromechanical equipment, including six variable-speed reversible Francis pump-turbines rated at 150 MW each, as well as six
asynchronous motor-generators. The scope included engineering, supply, site delivery, erection, supervision and commissioning in close collaboration with NDD staff.
With a storage capacity of 20 million kWh, equivalent to 20 GWh, Nant de Drance can store surplus electricity and release it during periods of higher demand. The plant can switch from full-power pumping to full-power generation in around five minutes, enabling rapid response to changes in electricity demand and supporting the resilience of the power system.