Located between the states of Minas Gerais and Goiás, the São Simão Hydropower Plant is a major asset in Brazil’s interconnected power system. With six generating units and an installed capacity of 1,710 MW, the plant supplies electricity to approximately 6 million homes and plays a strategic role in national power transmission and generation.
More than 45 years after GE Vernova installed the six turbines, the plant required a complete modernization to restore performance, improve reliability, and extend its operational life. GE Vernova is leading the project as consortium leader, delivering the full rehabilitation of the six Francis turbine-generating units, each with an installed capacity of 285 MW.
The modernization is introducing advanced technologies that significantly improve efficiency, availability, and long-term reliability, reinforcing São Simão’s role as a key generation asset in Brazil’s hydroelectric system.