Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / GetQuality Method
An index value.


GetQuality Method (IDataSamples)
Return the data value quality at a specific index.
Syntax
Function GetQuality( _
   ByVal index As System.Integer _
) As IDataQuality

Parameters

index
An index value.

Return Value

A data value quality.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also