Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / Times Method


Times Method
Return an array of data value times.
Syntax
Function Times() As System.Date()

Return Value

An array of data value times.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also