Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / HaveTimes Method


HaveTimes Method (IDataSamples)
Whether data value times are provided.
Syntax
Function HaveTimes() As System.Boolean

Return Value

True if this instance includes data value times.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also