Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / GetValue Method
An index value.


GetValue Method
Return the data value at a specific index.
Syntax
Function GetValue( _
   ByVal index As System.Integer _
) As System.Object

Parameters

index
An index value.

Return Value

A data value.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also