Add a General Comment for an Activity

Procedure

  1. Log in to Plant Applications Web Client.
  2. In the application navigation menu, select .
    The Open page appears.
  3. If the activity for which you want to add a comment is completed or skipped, select Completed.
  4. Select for the activity, and then select Add Comment.
    A window for entering comments appears.
  5. In the ADD GENERAL COMMENT box, enter a comment for the activity, and then select Save.
    The comment is added.
    Tip:
    Select Show Comments to access the comments for the activity.