Modify a Comment for a Variable

Procedure

  1. Log in to Plant Applications Web Client.
  2. In the application navigation menu, select .
    The Open page appears.
  3. Depending on the status of an activity, select Perform or In Progress for the activity associated with the variable.
    The page for entering data for the modifiable variables appears.
  4. Select , and then select Add/Edit Comment for a variable.
    A comments list in the window for entering comments for the selected variable appears.
  5. Select for the comment that you want to modify.
    The EDIT COMMENT box appears, displaying the comment.
  6. Modify the comment, and then select Save.
    The changes to the comment are saved.
    Note:
    The position of a comment in the comments list remains constant even after you modify the comment.