Add a Comment for a Variable

Procedure

  1. Log in to Plant Applications Web Client.
  2. In the application navigation menu, select .
    The Open page appears.
  3. Depending on the status of an activity, select Perform or In Progress for the activity associated with the variable.
    The page for entering data for the modifiable variables appears.
  4. Select , and then select Add Comment for a variable to add a comment.
    A window for entering comments for the selected variable appears.
  5. In the ADD NEW COMMENT box, enter a comment for the variable, and then select Save.
    The comment is added for the variable.
    Tip:
    If you are in the ADD NEW COMMENT box, then select Show Comments to access all existing comments entered for the variable.