Add Substitutions to BOM Item
Procedure
- Log in to Plant Applications Web Client.
-
Select
.
The BOM Editor page appears displaying the list of BOMs. -
Select the BOM for which you want to view the item details.
The Item Details section appears, displaying the available items.
-
Navigate to the Substitutions column, and select
Add Substitutions for the item to which you want to
add a substitution material.
Note:If the substitutions column is not displayed or hidden, then select Column Chooser
to add SUBSTITUTIONS column in the grid.
The Bom Formulation Details page appears. - In the Select product code drop-down list box, search for the product code and add the required product as a substitution material.
-
Enter QUANTITY required for substitute material to replace
full material of the main material. Also, select the appropriate UOM from the
UOM drop-down list box.
Note:The CONVERSION FACTOR field is updated automatically based on the quantity provided. If you choose to input the conversion factor field, then the QUANTITY field will be updated automatically.
-
Select Add.
Note:If you want to add more than one substitution, select
to add the substitutions for the BOM items.