Modify Items on a BOM
When the ECO Site parameter is enabled, you can update the BOM formulation with a Non-ECO Controlled material.
Before you begin
Procedure
- Log in to Plant Applications Web Client.
-
Select
.
The BOM Editor page appears displaying the list of BOMs. -
Select a BOM that you want to modify.
The BOM details window appears.
-
Select
to add or modify any BOM Formulation Item from the list.
The Edit BOM page appears. -
Update the required information in the following table:
Field Description ENTER BOM NAME/DESCRIPTION Displays the name for the new BOM Formulation. BOM FAMILY Select a BOM family from the list to enable and populate the Master BOM field. MASTER BOM Displays the name of the master BOM to which the new BOM Formulation belongs. MATERIAL Select the non-ECO controlled materials for which the BOM Formulation is created or available. You can select the Select All check box if you want to include all. Note:When the ECO Site parameter is enabled, the system does not display any ECO Controlled materials in the list. When the ECO site parameter is disabled, you can select both ECO Controlled material and a Non-ECO Controlled material.ENGINEERING UNITS Select appropriate engineering units (also known as Units of Measure) for the material selected in the previous field. REVISION Displays the revision number of the BOM Formulation. QUANTITY PRECISION Enter the valid number of decimal places for the value. Note:You can enter a precision up to 10 decimal places.QUANTITY Enter the quantity for the BOM formulation. This must follow the defined precision value. EFFECTIVE DATE Using the date picker, select the effective date and time of the formulation. Note:You can use a BOM formulation only from its effective date.EXPIRATION DATE Select the check box to enable the date picker. Using the date picker, select the date and time at which the formulation will expire. This field is optional. REASON Enter the reason for which the BOM formulation is updated. -
Click Update.
Any change to the list of BOM Formulation Items is saved.
- Select the < Back link if you want to navigate from an open BOM to the BOM Editor list screen.