Add BOM Item Properties

About this task

Use this procedure to update item specific properties.

Procedure

  1. Log in to Plant Applications Web Client.
  2. Select BOM Editor().
    The BOM Editor page appears, displaying the list of BOMs.
  3. Select the BOM for which you want to update item BOM properties.
    The Item Details section appears, displaying the available items.
  4. Click the Item Properties tab.
  5. To assign a property group to the BOM item, click Assign Property Group(s) ().
    The Assign Property Group(s) page appears and displays a list of available property groups.
  6. To assign the entire group to the BOM items, select the BomItem Import checkbox, then click Assign.
  7. On the Item Properties tab, click By Definition.
    The system displays all properties by definition.
  8. Based on the requirement, assign or unassign, or change the revision of the BOM items in the following table:
    Field Description
    DISPLAY NAME Displays the name of the property.
    MANDATORY Displays whether the property is mandatory or not.
    REVISION Displays the revision number of the property. You can change the revision number.
    UOM Displays the Units of Measure (UOM - also known as Engineering Units) of the property.
    Data Type Displays the data type of the property.
    Note:
    The Sync option is enabled when you assign or unassign a property group to a BOM item or change the revision. Clicking the Sync option, ensures that you retrieve all the latest changes.
    Note:
    Unlike BOM Properties, the By Values tab is not available for Item Properties. To add or update BOM item property values, navigate to the Item Details tab after adding the group where properties are displayed as columns. If a property is not visible, select the Column Picker and check the property to add it to the grid.
  9. Click Save.
    All the changes you made are displayed on the Item Details page as columns.