Add or Remove a Sample
About this task
Depending on the number of items in a material lot, the size of a sample is automatically calculated. If, however, you want to perform inspection on more samples, you can add more samples.
You can remove the samples that you have added. You cannot, however, remove the samples that are created automatically by the sampling engine.
Procedure
- If you want to add a sample, in the Inspection Criteria section, select
.
A new column is added in the table for another sample.Note:If you generated a sample of certain quantity of parts for periodic inspection, you will be able to add samples only for the remaining parts that were not selected for periodic inspection. For example, if you selected one part out of five parts for a periodic inspection, you can add only four samples and perform inspection. You will not be able to perform inspection on the part that was selected for periodic inspection. - If you want to remove a sample that you have added, in the Inspection Criteria section:The sample is removed.