Generate Samples for a Serialized Material

Before you begin

Access the receiver for which you want to generate samples. You can generate samples only for a material lot for which inspection tests are defined in Plant Applications Administrator (indicated by ).

Procedure

  1. In the left pane, under the receiver, select the material for which you want to generate samples.
    The Edit Traceability section appears.
  2. In the Add subsection, provide values as described in the following table.
    BoxDescription
    PREFIXThe prefix of the item's serial number. The value can be in alphanumerical format with any special characters. For example AV-.
    SUFFIX The suffix of the item's serial number. The value can be in alphanumerical format with any special characters. For example -2021.
    STARTING SERIAL The serial number of the first item in the material lot. This value is used to number each item in the material lot. For example, if you enter PVC Pipe 01, the items in the material lot are numbered PVC Pipe 01, PVC Pipe 02, PVC Pipe 03, and so on.

    A value is required.

    Note:
    The Starting serial can be either alphabets or numbers. No special characters are allowed.
    SERIAL COUNTThe total number of items in the material lot.
    Note:
    The validation of duplicate serial numbers happens along with the concatenation of the string that you entered.
  3. As needed, enter values in the remaining fields.
  4. Select Add to Table.
    Serial numbers are generated for all the items in the material lot, and appear in the table in the Edit subsection. The fields in the Add subsection are disabled.
  5. In the grid, perform the following:
    1. Enter a number in the LOT NUMBERS column.
    2. Enter the quantity in the QTY column.
    3. If you want to generate samples for a periodic inspection, ensure to select the check box that is available under Periodic Inspection column.
      Note:
      Once you select a part and its quantity for periodic inspection, you cannot change the quantity or the inspection type for that lot.
  6. Select Save.
    Changes to the serial numbers are saved.
    Note:
    You can continue to change the serial numbers until the inspection begins. After you enter the inspection criteria, you cannot change the serial numbers.
  7. Select Generate Samples.
    Samples are generated for the serialized material lot and appear in the Inspection Criteria section. The size of the sample is calculated based on the size of the lot. The status of the receiver changes to awaiting inspection (indicated by ).

What to do next

Perform inspection on the samples. If needed, you can add more samples.