Generate Samples for a Non-Serialized Material
Before you begin

Procedure
- In the left pane, under the receiver, select the material for which you want to generate samples.The Edit Traceability section appears.
- If you do not want to split the lot:
- If you want to split the lot:
- As needed, enter values in the remaining fields.
-
Select Save.
Changes to the lot are saved.Note:You can continue to change the lots until the inspection begins. After you enter the inspection criteria, you cannot change the lots.
-
Select Generate Samples.
The Generate Samples button is enabled only if the sum of the quantities of all the sublots is equal to the total number of items in the lot.Samples are generated for the lot or each sublot and appear in the Inspection Criteria section. The size of the sample is calculated based on the size of the lot or sublot. The status of the receiver changes to awaiting inspection (indicated by
).