What is Condition-Based Maintenance & How Can it Be Leveraged as Part of a Holistic Asset Performance Management Strategy?

Author Sticky

Rahul Vijayaraghavan

Product Marketing Manager

GE Vernova’s Software Business

Rahul is part of GE Vernova’s Power Energy Resources marketing team providing strategic support for applications within the Asset Performance Management portfolio. He has over 10 years of functional expertise in market and competitive intelligence including previous stints with the Central Marketing team and Flight Analytics at GE’s former Aviation business (now GE Aerospace). 

Jan 08, 2026 Last Updated
11 Minute read

Key Takeaways

  • Condition-based maintenance is a preventative maintenance strategy that focuses on the actual condition of the asset rather than a set time-based schedule.
  • Condition-based monitoring is expanding to include cameras, robotics, infrared imaging and ultrasounds in addition to operator rounds.
  • Organizations performing condition-based maintenance are exploring combining data from physics-based models with machine learning models.
  • Unlike predictive maintenance, condition-based maintenance is performed on an as-needed basis.
  • The benefits of condition-based maintenance include increased reliability and uptime, maintenance cost savings, increased operational efficiency, and increased safety and compliance.
  • Successful condition-based maintenance programs typically begin with defining the scope and criticality that will be included in the program.
Prefer to listen?

Stream our audio version

00:00/00:00

Introduction

According to research from MarketsandMarkets, the condition-based maintenance market is expected to grow from $10.6B in 2024 up to $47.8B by 2029. This increase is expected due to energy organizations working to meet production and energy transition requirements by better monitoring assets to help drive more efficient operations.

So, what are the key elements of condition-based maintenance? What are the potential benefits for your organization? How is condition-based maintenance evolving?

Let’s check it out.

What is Condition-based Maintenance?

Condition-based maintenance is a preventative maintenance strategy that focuses on the actual condition of the asset rather than a predetermined maintenance schedule. Condition-based maintenance is often times included as part of a predictive maintenance strategy, that relies on various datapoints to determine a true condition of the asset(s) being monitored.

Today, condition-based maintenance programs can draw insights from more data than ever before. This can include data inputs from sensors, operators, images, robotics, and satellite imagery based on industry. Organizations are able to use this aggregated data for subject matter experts (SMEs) to make decisions, leverage machine learning (ML) for simple analysis of asset changes, or artificial intelligence (AI) in the form of predictive analytics to develop an overall risk profile of assets being monitored with condition-based programs.

How is Condition-based Maintenance Different than Predictive Maintenance?

While both condition-based and predictive maintenance are focused on reducing asset failures, increasing production, and extending asset lifespans, there are key differences.
  1. Condition-based is performed on an as-needed basis: condition-based maintenance relies on data being collected to be able to properly dispatch teams as appropriate. This is a designed process that helps organizations to better manage work, focus on critical problems, and ultimately maintain uptime. On the other hand, predictive maintenance is a proactive approach to maintenance, mostly used on highly critical assets, to help identify the potential time when an asset may fail or drop below expected operating parameters.
  2. Condition-based requires more data points: condition-based monitoring is far more than running analytics on time series or sensor data. Organizations performing condition-based maintenance are collecting test, inspection, image, and other real-time data from the field to create a health index. Predictive often relies more on sensor and historian data to generate alerts that may not consider elements from condition-based programs.
Each of these approaches have the potential to bring immense value to organizations. In fact, some of the most highly performant asset-intensive organizations employ both condition-based and predictive maintenance depending on asset criticality or importance to production.

Benefits of Condition-based Maintenance

There are several benefits to condition-based maintenance. As a leader in the asset performance management space, GE Vernova has seen the following benefits by using a condition-based approach:
  • Increased reliability and uptime
  • Increased O&M cost savings
  • Increased operational efficiency
  • Increased safety and compliance
  • Increased data cleanliness and fidelity
  • Positive impacts on sustainability and emissions
Furthermore, industries across the energy ecosystem can reap the benefits of a holistic condition-based maintenance program. Listed below are some examples of operators using GE Vernova’s APM Health condition-based maintenance solution to see tangible outcomes.
  • Power & Renewables: Xcel Energy, a leading utility company in America, uses GE Vernova’s APM solution across its mixed-fuel fleet, which includes ~10,000MW fleet capacity of natural gas turbines and wind/solar/hydro respectively that fall into the Asset Performance Management program and digital transformation scope. Specific to using GE Vernova’s APM Health, they built an asset health score and health index using data from users, operator rounds, engineering rounds, and testing. (Learn More)
  • Oil and Gas: HMEL, an integrated refining and petrochemical company in India, uses GE Vernova’s APM solution to ingest and analyse critical information from Policies, ODR Rounds, APM Health module and other applications to improve reliability and availability of the equipment. They have seen a significant MTBF improvement specifically for pumps and reciprocating compressors. (Learn More)
  • Chemical: Eastman Chemical, an independent specialty chemicals producer in America, integrates GE Vernova’s APM Health and Rounds Pro mobile application into their risk-based operational monitoring (RBOM) program to improve recommendation processing – they now achieve 1200-1400 recommendations per quarter with ~90% quality ratings. (Learn More)
  • Packaging: SIG, a manufacturer in the packaging industry, uses GE Vernova’s Plant 360 Asset Health Monitoring service (includes GE Vernova’s APM Health & APM Strategy applications) to minimize unplanned downtime and keep output at a maximum. One of SIG’s customers saw a 20% reduction in unplanned downtime in just one year after implementation. (Learn More)

Potential Pitfalls of Condition-based Maintenance

It’s clear that a condition-based approach to maintenance has the potential to deliver real impact to an organization. However, it’s also evident from GE Vernova’s deep experience in these areas, that there are some key elements that could create potential friction that will need to be mitigated:

Poor data quality and instrumentation

When sensor coverage or other instrumentation is spotty, organizations may get noise or inconsistencies from data. To help mitigate, it is recommended to start with a criticality analysis of assets and align these programs to the top 25% of assets.

Siloed data

With the increasing requirements of data that needs to be leveraged in condition-based maintenance, ultimately there is a chance siloes will be identified or created. In order to help manage this, organizations require an ingestion strategy that spans IT, OT, and ET systems.

Unclear business case

As operators look to get investments to perform advanced maintenance, it is often difficult to determine the right use case. This leads to the potential of not delivering on the promised outcomes. To address this, it is critical that OT and IT teams are aligned on the scope of the program, technology required and expected return.

Change management

Many in asset intensive organizations have deep subject matter expertise and have been performing maintenance at a high-level for many years, this may lead to hesitancy to adopt new technology. To avoid this concern, it is important to keep SMEs involved in the program, create a clear adoption plan and document value of the condition-based program.

How do you Deploy Condition-based Maintenance?

Successful condition-based maintenance programs typically begin with defining the scope and criticality that will be included in the program, often these are asset classes that impact safety, cost or production goals. Once selected, it’s important to validate the data readiness of the selected asset classes, including aligning the assets to proper asset hierarchies to allow for clean data to flow. After the data is determined to be validated, organizations can then integrate existing tools or deploy new tools to connect plant-level data. Once completed, users can then create proper tie-ins to other systems such as CMMS or EAM and begin to fine-tune maintenance practices based on plant data.

Once condition-based maintenance is deemed successful at the plant level, organizations have the opportunity to scale programs across the enterprise. From the first plant, organizations can develop a playbook that can be repeated and aligned with corporate asset strategies, such as Failure Modes and Effects Analysis (FMEA) and Reliability Centered Maintenance (RCM). This can enable users to expand the coverage of condition-based programs to more assets and allow for the ability to benchmark data from individual plants against one another to determine best maintenance practices.

Conclusion:

Condition-based maintenance, when done properly, has the ability to make a major difference for asset-intensive organizations. From helping to align SMEs to assets, to deploying AI/ML for advance insights, condition-based maintenance helps to generate a foundation for organizations to get the most out of their assets.

Author Section

Author

Rahul Vijayaraghavan

Product Marketing Manager
GE Vernova’s Software Business

Rahul is part of GE Vernova’s Power Energy Resources marketing team providing strategic support for applications within the Asset Performance Management portfolio. He has over 10 years of functional expertise in market and competitive intelligence including previous stints with the Central Marketing team and Flight Analytics at GE’s former Aviation business (now GE Aerospace).