Your choice of business systems has a direct impact on manufacturing efficiency

Author Sticky

Malene Andersen

Marketing Specialist – Product Marketing

Manufacturing

Malene has 15+ years of experience in marketing and communication, specialising in driving business growth through clear strategy and compelling storytelling. She brings over a decade of experience in industrial automation, with a focus on product marketing for Proficy Scheduler.

Holding a Master of Arts degree in Culture and Communication from the University of Odense, Denmark, Malene excels at translating complex technical concepts into clear, actionable insights. Her deep understanding of production planning enables her to connect technology with real business value, helping manufacturers improve efficiency and performance.

May 26, 2026 Last Updated
10 Minutes Read

Production planning is at the heart of manufacturing operations. It determines how effectively companies can utilize capacity, manage materials, coordinate resources, and deliver products on time.

In modern manufacturing environments, production planning is no longer a static scheduling exercise. It is a continuous decision-making process shaped by constant change, including machine availability, material constraints, shifting priorities, and unexpected disruptions.

Because of this, the planning and scheduling tools a company uses have a direct impact on shop floor visibility, operational control, and on-time delivery performance.

Many manufacturers are therefore re-evaluating whether traditional planning tools such as ERP modules, spreadsheets, and manual coordination are sufficient for today’s level of operational complexity.

Production planning today: increasing complexity and constant change

Manufacturing environments have become significantly more dynamic. Production planners are expected to manage:
  • Frequent changes in customer demand
  • Limited and variable production capacity
  • Material shortages and supply delays
  • Equipment downtime and maintenance
  • Competing production priorities
In many organizations, planning and scheduling are still handled through ERP systems, Excel files, and manual coordination between departments. These approaches are not designed for the level of operational complexity found in modern manufacturing environments, which often results in fragmented visibility and a gap between planned activities and actual shop floor execution. As a result, planners spend increasing time reacting to disruptions instead of proactively managing production flow.

Where production planning breaks down

When planning is not fully aligned with operational reality, several challenges typically emerge:
  • Lack of real-time shop floor visibility
  • Frequent schedule deviations
  • Limited understanding of production constraints
  • Delayed identification of bottlenecks
  • Increased work-in-progress (WIP)
  • Reactive firefighting instead of structured control
The core issue is not a lack of data. Most manufacturers already generate large volumes of production data through ERP systems, shop floor systems, and other digital tools that capture transactions, material movements, and operational events across the production environment.

The challenge is not data availability, but data alignment. Planning, execution, and shop floor operations are often not fully connected in a dynamic, coordinated system, making it difficult to translate available data into actionable production decisions.

Why ERP-based planning is often not enough

ERP systems play a critical role in manufacturing operations, particularly in finance, procurement, inventory, and high-level planning.

However, when it comes to detailed production scheduling, ERP systems are typically limited in flexibility and depth. They are often not designed to handle:
  • Real-time rescheduling of orders
  • Complex production constraints
  • Dynamic prioritization
  • Detailed shop floor sequencing
  • Continuous operational changes
This creates a gap between enterprise planning and actual production execution on the shop floor.

Why specialized production scheduling software is required

To manage this complexity, manufacturers increasingly rely on specialized production scheduling software designed specifically for operational planning and execution.

This is where Proficy Scheduler comes in: a purpose-built production planning solution that helps manufacturers move from fragmented, reactive planning to structured, data-driven scheduling.

Instead of relying on disconnected tools and static plans, Proficy Scheduler provides a single, dynamic view of production that reflects real operational conditions across the shop floor.

How Proficy Scheduler improves production planning

Proficy Scheduler is designed to support production planners in managing variability, constraints, and continuous change in real time.

It enables manufacturers to:
  • Maintain a continuously updated production schedule
  • Gain real-time visibility into order progress and flow
  • Understand dependencies between operations, materials, and resources
  • Identify bottlenecks and constraints earlier
  • Simulate the impact of changes before execution
  • Quickly adjust schedules when disruptions occur
This shifts production planning from a reactive activity to a controlled and proactive decision-making process.

From reactive planning to controlled production flow

With traditional approaches, production teams often operate reactively responding to issues after they appear on the shop floor.

With a structured scheduling system like Proficy Scheduler, planning becomes aligned with actual production constraints and execution of reality.

This enables manufacturers to achieve:
  • More predictable production flow
  • Stronger coordination between planning and execution
  • Reduced manual intervention and firefighting
  • Improved decision-making based on real-time operational data
The result is not only improved efficiency, but also a more stable and controllable production environment.

Production scheduling in a volatile manufacturing environment

Manufacturers today operate in an environment defined by constant change. Production scheduling must therefore be flexible, responsive, and continuously optimized.

Proficy Scheduler is designed for this reality and helps manufacturers manage disruptions such as:
  • Machine downtime
  • Material shortages
  • Priority changes
  • Urgent customer orders
  • Supply chain delays
Instead of treating disruption as an exception, it becomes an integrated part of the planning process.

Integrating Proficy Scheduler with existing systems

Proficy Scheduler is not designed to replace ERP systems, but to complement them.

ERP continues to manage enterprise-wide processes, while Proficy Scheduler adds a dedicated operational layer for detailed production scheduling and execution control.

This integration ensures:
  • Alignment between business planning and shop floor execution
  • Consistent and up-to-date production data
  • Reduced manual coordination between departments
  • Faster and more informed responses to change
Together, they form a more complete and connected manufacturing planning architecture.

Improving production planning with Proficy Scheduler

Effective production planning is essential for manufacturing performance, operational efficiency, and delivery reliability.

However, as manufacturing complexity increases, traditional tools often struggle to maintain alignment between planning and reality.

By introducing a specialized production scheduling solution such as Proficy Scheduler, manufacturers can move toward structured, real-time scheduling that reflects actual shop floor conditions.

This leads to:
  • Improved shop floor visibility
  • More reliable and stable production schedules
  • Faster response to disruptions
  • Reduced operational complexity
  • Stronger on-time delivery performance
Ultimately, Proficy Scheduler enables manufacturers to transform production planning from a reactive process into a controlled, transparent, and data-driven capability.

Author Section

Author

Malene Andersen

Marketing Specialist – Product Marketing
Manufacturing

Malene has 15+ years of experience in marketing and communication, specialising in driving business growth through clear strategy and compelling storytelling. She brings over a decade of experience in industrial automation, with a focus on product marketing for Proficy Scheduler.

Holding a Master of Arts degree in Culture and Communication from the University of Odense, Denmark, Malene excels at translating complex technical concepts into clear, actionable insights. Her deep understanding of production planning enables her to connect technology with real business value, helping manufacturers improve efficiency and performance.