Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class


ConnectionProperties Class Properties

For a list of all members of this type, see ConnectionProperties members.

Public Properties
 NameDescription
Public Property Maximum amount of time to close a connection before timing out. Default value is 1 minute.  
Public Property Maximum amount of time before an inactive connection will time out. Default value is 10 minutes.  
Public Property The maximum number of objects (including array elements) to serialize or deserialize. Default value is 1M.  
Public Property Maximum size for a received message in bytes. Default is 1M.  
Public Property Maximum amount of time to attempt to open a connection before timing out. Default value is 1 minute.  
Public Property A matching user password.  
Public Property Maximum amount of time to receive before timing out. Default value is 1 minute.  
Public Property Whether to enable reliable sessions. Default value is false.  
Public Property Maximum amount of time to send a request before timing out. Default value is 1 minute.  
Public PropertyA method of validating a security certificate on a Historian server.

Default is CertificateValidationMode.ChainTrust, a certificate is considered valid if the chain builds to certification authority in the trusted root store.

Use CertificateValidationMode.None, to connect to a Historian server secured by a self-signed certificate (out-of-the-box configuration).

 
Public PropertyA fully qualified host name of a Historian server. Due to security identity checks, it is not possible to connect simply via server IP address.

Default is local server if unspecified.

 
Public Property A name of a user account with access to the server. If unset the current Windows user is used for authentication.  
Public Property Maximum array length returned by the reader. Default value is 1M.  
Public Property Maximum bytes consumed by the reader at one time. Default values is 4K.  
Public Property Maximum nested XML node depth. Limits the XML nested node depth. Default value is 32.  
Public Property Maximum size of character data in a reader's NameTable. Default value is 16K.  
Public Property Maximum length of a string returned by the reader. Default values is 8K.  
Top
See Also