Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / OpenTimeout Property


OpenTimeout Property
Maximum amount of time to attempt to open a connection before timing out. Default value is 1 minute.
Syntax
Public Property OpenTimeout As System.TimeSpan
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also