Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / XmlReaderQuotaMaxDepth Property


XmlReaderQuotaMaxDepth Property
Maximum nested XML node depth. Limits the XML nested node depth. Default value is 32.
Syntax
Public Property XmlReaderQuotaMaxDepth As System.Integer
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also