Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / InactivityTimeout Property


InactivityTimeout Property
Maximum amount of time before an inactive connection will time out. Default value is 10 minutes.
Syntax
Public Property InactivityTimeout As System.TimeSpan
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also