Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / ReliableSessionEnabled Property


ReliableSessionEnabled Property
Whether to enable reliable sessions. Default value is false.
Syntax
Public Property ReliableSessionEnabled As System.Boolean
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also