GridOS for Transmission

GridOS® for Transmission

From Siloed Systems to
One Transmission Grid.

GridOS for Transmission is GE Vernova’s unified grid orchestration solution for managing the transmission network as one system.  
Transmit more power, respond faster, and operate the grid securely at scale by unifying real-time operations, grid balancing, capacity management, forecasting, and network intelligence. 

GridOS for Transmission

Overview

The grid is being pushed beyond its operating model. 

Electrification, renewable intermittency, extreme weather, and new load patterns are driving volatility in transmission networks, and grid operations can’t keep pace. Disparate tools, delayed visibility, and conservative assumptions limit usable capacity. Utilities are not constrained by infrastructure alone, but by the way they understand and operate the grid. 

A new operating model is required.

Managing today’s transmission grid demands a fundamental shift:
  • From static limits to dynamic capacity awareness.
  • From siloed tools to coordinated system-wide intelligence.
  • From delayed visibility to continuous, real-time awareness.
  • From reactive actions to predictive and confident decision-making. 
GridOS for Transmission

GridOS for Transmission:

Helping modernize the transmission grid. 

GridOS for Transmission
GE Vernova

Introducing GridOS for Transmission  

A unified software solution that helps utilities operate the transmission grid as one coordinated system. 
It brings critical capabilities into a single, interoperable environment: 

  • Real-time operations to monitor and control the grid. 
  • Capacity management to unlock transmission headroom.
  • Stability monitoring to track system dynamics and risks. 
  • Forecasting to anticipate load and renewable variability.
  • Network intelligence to connect insights across the grid.
  • Built on a federated data foundation that syncs various transmission systems into one source of truth. With GridOS for Transmission, utilities can:

  • See the true operating state of the grid in real time.
  • Understand available capacity under current and forecasted conditions.
  • Detect stability risks early and act before they escalate.
  • Make faster, coordinated decisions across operations and planning.

GridOS for Transmission: Applications 

GridOS for Transmission brings together a set of core applications and extensible capabilities to support real-time operations, capacity optimization, and evolving grid requirements. 
GridOS for Transmission: Applications 
AEMS
Provides the operational core for real-time monitoring, control, and secure transmission grid operations. Enables state estimation, contingency analysis, and coordinated control actions across the network to maintain reliable and efficient system performance. 
GridOS for Transmission: Applications 
GridOS DDLR
Delivers digital dynamic line ratings using real-time weather conditions and forecasts, enabling operators to safely increase transmission capacity, reduce congestion, and optimize power flows while maximizing use of existing infrastructure. 
GridOS for Transmission: Applications 
GridOS WAMS
Provides synchronized, high-resolution monitoring of grid dynamics, enabling early detection of oscillations, angle instability, and system stress. Supports timely corrective actions to maintain stability and ensure secure transmission system operations under changing conditions. 
GridOS for Transmission: Applications 
GridOS Forecasting
Enables accurate forecasting of load and renewable generation, helping operators anticipate variability and align operational decisions with reality. Supports proactive planning, improved dispatch strategies, and overall more efficient transmission management at scale. 
GridOS for Transmission: Applications
GridOS Visual Intelligence
Uses image analytics to monitor transmission asset health, detect anomalies, and enhance situational awareness. Enables operators to identify issues beyond traditional system data and improve visibility across physical grid infrastructure and operations. 

Available as an add-on capability to extend visibility across physical grid infrastructure. 
GridOS for Transmission: Applications 
GridOS Markets
Supports market operations by enabling bidding, scheduling, and settlement processes aligned with real-time grid conditions.

Available as an add-on capability to enable integrated market participation aligned with real-time grid operations. 

How GridOS for Transmission works 

GridOS for Transmission brings together real-time operations, system intelligence, and advanced analytics into a unified operational environment, enabling utilities to manage capacity, stability, and grid behavior as one coordinated system. 

At its core is AEMS, connected to a growing set of GridOS applications that extend system intelligence across the network. 

- AEMS (Operational Core): Executes real-time monitoring, control, and grid operations. 
- GridOS Applications (Intelligence Layer): Extend capabilities across capacity, stability, forecasting, and visual intelligence. 
- Data Fabric & Connect (Data Foundation): Enables seamless integration, real-time data flow, and interoperability across systems. 

Together, they create a continuous decision loop, where real-time insights, predictive intelligence, and coordinated actions operate within a single, connected system. 

GridOS for Transmission works 

Speak with a utility software expert about how GridOS for Transmission can help ensure a reliable
and resilient sustainable-energy grid.

“Thank you for getting in touch!” 

We’ve received your message, One of our colleagues will get back to you soon. Have a great day! 
Resources

Blogs

Videos

FAQs

FAQs

What is GridOS for Transmission?
GridOS for Transmission is a modern operating framework that helps utilities coordinate awareness, capacity, stability, resilience, and operational workflows across the transmission network. It brings together operational intelligence from multiple domains into a more connected and coordinated operating environment.

Is GridOS for Transmission a replacement for EMS?
No. GridOS for Transmission is not a replacement for EMS. EMS remains at the operational core of the control room. GridOS for Transmission builds the foundation by connecting operational intelligence, workflows, and applications across the broader transmission ecosystem.

What challenges does GridOS for Transmission help address?
GridOS for Transmission is designed to help utilities address challenges such as increasing grid complexity, congestion, renewable integration, data center load growth, stability risks, extreme weather events, aging infrastructure, and the need to maximize the utilization of existing assets.

How does GridOS for Transmission differ from traditional transmission management systems?
Traditional systems are often focused on individual operational functions. GridOS for Transmission focuses on coordinating intelligence and decision-making across operational domains, helping utilities move from managing individual systems to operating the grid as one connected system.

How does GridOS for Transmission support transmission operators?
GridOS for Transmission helps operators work from a more coordinated operational context by connecting information from multiple systems and domains. This can help reduce decision latency, improve situational awareness, and support faster, more informed operational decisions.

What is the core operational competencies of GridOS for Transmission?
GridOS for Transmission is built around four operational competencies:

- Network Awareness
- Capacity Management
- Stability Management
- Grid Resilience

Together, these competencies help utilities improve visibility, utilization, reliability, and preparedness across transmission operations.

Can utilities adopt GridOS for Transmission incrementally?
Yes. Utilities can evolve toward GridOS for Transmission progressively. Organizations can start with a modern operational foundation and expand capabilities over time based on business priorities, operational challenges, and modernization goals.

How does GridOS for Transmission help improve asset utilization?
GridOS for Transmission helps utilities combine operational awareness, capacity intelligence, and planning insights to make better use of existing transmission infrastructure. This can help increase transfer capability, manage congestion, and defer unnecessary capital investments.

How does GridOS for Transmission support grid resilience?
GridOS for Transmission helps utilities strengthen preparedness, response, and recovery by bringing together operational awareness, stability intelligence, restoration workflows, and resilience-focused applications into a coordinated operational framework.

How does GridOS for Transmission support the transition toward a more dynamic grid?
As transmission systems become more dynamic due to renewables integration, electrification, and evolving load patterns, GridOS for Transmission helps utilities connect operational intelligence across the grid and adapt more effectively to changing conditions, supporting more coordinated and predictive operations.