GridOS® DDLRDynamic line rating software for utilities.GE Vernova’s dynamic line rating software, GridOS® Digital Dynamic Line Rating (DDLR), brings capacity intelligence to transmission networks. Create a more consistent capacity context for informing decisions across the transmission network.Download the solution paper GridOS® DDLR Overview The grid may have more capacity than its static rating suggests.Electricity demand is growing. Generation patterns are changing. Congestion is affecting locations where additional transmission infrastructure can take years to build. Yet, the capacity of the existing infrastructure is not always static.Environmental and operating conditions can impact how much power a transmission infrastructure can safely carry. Electrical conductor is only part of the equation. The equipment elsewhere along the electrical path can ultimately determine the usable capacity of a facility.The challenge is not simply finding more line capacity. Utilities need to know what capacity is available, what is limiting it, and how that capacity may change over time. The available capacity changes with the decision What limits capacity?Understand conductor, equipment, and facility constraints that determine usable capacity. What capacity could be available?Explore transmission changes across different scenarios What will be available ahead?Anticipate how the available capacity may change over upcoming hours and days. What can be safely used now?Bring the current capacity information into operational decisions as conditions change. GridOS® DDLR brings intelligence into utility decisions.GridOS DDLR is a software-based dynamic line rating solution for capacity decisions, designed to help utilities use existing transmission infrastructure effectively while respecting operating limits.It brings together four complementary capacity capabilities:FACILITY RATING MANAGEMENTUnderstand the capacity of the complete electrical path and identify equipment that may constrain the facility.STUDY & SCENARIO ANALYSISExplore how capacity could change under different network, asset, and environmental scenarios.FORECAST FACILITY RATINGSLook ahead at the expected capacity to support the upcoming operational and planning decisions.DYNAMIC FACILITY RATINGSContinuously assess the transmission capability as environmental and operating conditions change. See capacity differently. Use the network efficiently. Unlock available capacityIdentify additional transmission headroom when conditions allow and make better use of the infrastructure already in service. Manage congestionBring the current and forward-looking capacity information into decisions across constrained transmission corridors. Plan generation and load integrationUnderstand how the changing transmission capability affects the ability to accommodate new generation and growing demand. Make better infrastructure decisionsDistinguish where additional capacity may be available from where physical infrastructure remains the limiting factor. Plan with greater visibilityAnticipate the changing capacity conditions for congestion management, outage planning, and upcoming operations. Operate within facility limitsConsider transmission line capability together with relevant equipment constraints when determining the usable capacity. Load More Capacity intelligence at network scale 33%GridOS DDLR can increase line capacity by up to 33%. 250xCompared to sensor-based solutions, GridOS' digital dynamic line rating can offer an investment reduction of up to 250 times. 10DAYSHourly forecast capacity visibility Scale capacity visibility without instrumenting every line.GridOS DDLR can calculate dynamic capacity without requiring sensors across every monitored transmission line, helping extend capacity assessment to a broader portion of your network.Already invested in sensors?Those investments do not have to be replaced. Utilities can use strategic assets where direct measurement makes sense while deploying GridOS DDLR to widen capacity intelligence.Explore Sensor Data Integration Bring capacity intelligence into the systems where decisions happen. GridOS DDLR is designed to work with existing utility environments.Capacity information can be exchanged with EMS/ADMS, planning, and enterprise systems through standard interfaces, enabling the use of DDLR insights within established workflows rather than creating another isolated source of information.Deploy in the cloud or on-premises based on utility IT, cybersecurity, and regulatory requirements. Start with the corridors or capacity challenges that matter the most, then expand with evolving operational needs. Additional resources Capacity Intelligence for Transmission NetworksWhy understanding transmission capacity is becoming a continuous planning and operational decision.Read article Unlock Transmission Capacity with GridOS DDLRA deeper look at how GridOS DDLR turns changing conditions into actionable capacity information.Download the Solution Paper DDLR in PracticeHear how PG&E is applying digital line ratings to real transmission capacity challenges.Watch webinar Load More Resources Blogs Videos Get in TouchGet in Touch Connect with a utility software expert about how GridOS can help ensure a reliable and resilient sustainable-energy grid.Fill out the form below. Thank you for getting in touch! We’ve received your message, One of our colleagues will get back to you soon. Have a great day!