Skip to main content
Revolutionizing Lower-Carbon Power Generation with Carbon Capture at Net Zero Teesside Power
Feature story
Concept to Reality

Revolutionizing Lower-Carbon Power Generation with Carbon Capture at Net Zero Teesside Power

3 min read

Share

GE Vernova, together with Technip Energies and their construction partner Balfour Beatty, are preparing to build a giant power plant with carbon capture and storage (CCS) in Teesside, an industrial hub in northeast England. Net Zero Teesside Power (NZT Power) is expected to be the world’s first large-scale gas power plant designed with carbon capture built right into its core.

One of a portfolio of carbon capture technologies supporting the energy transition — such as direct air capture, a more recent innovation that pulls CO2 out of the atmosphere — this project is focused on capturing emissions before they even leave the plant.

Audio file
00:00/00:00
Hongtao Li, Carbon Capture System Integration Leader at GE Vernova

 

 

 

Working with Technip Energies and Shell Catalysts & Technologies, GE Vernova will supply all major equipments of the power island for the plant — which is a joint venture between BP and Equinor — including a 9HA.02 gas turbine and accompanying steam turbines and generators, as well as an exhaust gas recirculation (EGR) system that allows the operator to boost the efficiency of CCS.

 

When it begins operation, the project is expected to generate more than 740 megawatts of reliable and flexible electricity — roughly the equivalent needed to meet the annual electricity requirements of more than one million UK homes.

“The U.K. is on the path to net zero, and GE Vernova is rising to the challenge. We are integrating advanced CCUS technology with GE Vernova’s high-efficiency 9HA gas turbine to generate ultra-low-carbon power.”

Jeremee Wetherby

GE Vernova’s carbon solutions leader

 

Audio file
00:00/00:00
Hongtao Li, Carbon Capture System Integration Leader at GE Vernova 

 

Audio file
00:00/00:00
Mike Fryer, Early Works Construction Manager at Technip Energies 

Find out more about how GE Vernova is playing a key role in writing the blueprint for large-scale carbon capture and storage here.

“The fleet of commercially available construction cranes in the region are the right fit for GE Vernova’s more compact workhorse, and wouldn’t be able to handle larger turbines.”

Lukasz Siwik

Engineering Manager

 

Continue with the next story — New Generation: Upskilling Vietnam’s Workforce for the Renewables Age — and explore the full Concept Becomes Reality series.

 

Forward-Looking Statements
This article contains forward-looking statements, which provide current expectations based on certain assumptions. Except as required by law, we disclaim any obligation to update these statements.