- Powered by GE’s portfolio of renewable steam offerings, Kamisu Biomass Power Generation plant will run on 100% biomass to generate 50 MW of reliable and dependable electricity
 - GE Steam Power to provide Hitachi Zosen Corporation of Japan with integrated power package including steam turbine generator and boiler as well as air quality control systems
 - Builds on GE’s 100 years of experience providing efficient and reliable steam power technology across a range of fuel sources
 
Baden, SWITZERLAND — February 5, 2020 — GE (NYSE:GE) announced today that it will provide its renewable steam technology for the high efficiency Kamisu Biomass Power Generation plant in Japan. In a deal signed with Hitachi Zosen Corporation, acting as the project’s engineering, procurement and construction (EPC) contractor, GE Steam Power will design, manufacture and supply all core components of the power block for the project through an integrated power package including the steam turbine generator as well as the boiler with its air quality control systems.
Located in Kamisu City, Ibaraki Prefecture in Japan, the Kamisu Biomass Power Generation plant will use 100 percent biomass comprised of palm kernel shells and wood pellets to generate 50 megawatts (MW) of reliable and dependable power to the national grid. The plant will be equipped with GE’s low-NOx circulating fluidized bed (CFB) boiler, a high-efficiency dust-removal fabric filter and a reheat steam turbine with its generator.
“GE Steam Power’s involvement in the Kamisu Biomass Power Generation project demonstrates our commitment to applying proven steam power technology to lower carbon uses and supporting the use of more renewable fuel sources like biomass,” said Michael Keroulle, CEO of GE Steam Power. “Building on our proven track record of delivering steam power technology and project management capabilities for plants around the world, our integrated offering will help Hitachi Zosen achieve its high efficiency and reliability performance low-carbon objectives.”
The plant is scheduled to start commercial operation in July 2023.
###
About GE Steam Power
GE Steam Power is helping customers achieve their cleaner power generation objectives with a broad portfolio of technologies that can be applied to new-built plants and the installed base across a range of fuel sources including nuclear, coal, oil, biomass, solar and municipal waste. As today’s #1 steam power franchise with more than 30% of the world’s steam turbine installed capacity, 50% of the world's steam turbines operating in nuclear power plants and 30% of the world’s boilers, GE Steam Power technology is delivering solutions that optimize the reliability, affordability, flexibility and environmental impact of steam power plants all over the world.
 
end