Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / Instance Property


Instance Property
Returns the singleton Tracer instance.
Syntax
Public Shared ReadOnly Property Instance As Tracer
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also