Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / TraceOff Property


TraceOff Property
Gets whether tracing to file is currently disabled, level set to Off.
Syntax
Public Shared ReadOnly Property TraceOff As System.Boolean
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also