Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / Level Property


Level Property
Gets or sets the level that controls the types of messages recorded to file. Available levels include: Error, Warning, Info, Verbose and Off.
Syntax
Public Shared Property Level As System.Diagnostics.TraceLevel
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also