Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / WriteLine Method / WriteLine(String,Object) Method
A subject string to write.
A value to write.


WriteLine(String,Object) Method
Write the supplied subject and value to System.Diagnostics.Trace and to all registered listeners such as file and/or console.
Syntax
Public Overloads Shared Sub WriteLine( _
   ByVal subject As System.String, _
   ByVal value As System.Object _
) 

Parameters

subject
A subject string to write.
value
A value to write.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also