Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / WriteLine Method / WriteLine(Object,TraceLevel) Method
A value to write.
A trace level.


WriteLine(Object,TraceLevel) Method
Write a message value to System.Diagnostics.Trace depending on supplied trace level.
Syntax
Public Overloads Shared Sub WriteLine( _
   ByVal value As System.Object, _
   Optional ByVal level As System.Diagnostics.TraceLevel _
) 

Parameters

value
A value to write.
level
A trace level.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also