Control Data Updates
These functions allow users to control how data is displayed and refreshed.
- View Real-time Updates: Displays real-time values and units as they update.
- Pause the Data Flow: Helps you analyze a specific moment without new data appearing on the chart.
- Reset the Trend Chart: Revert all changes made to the trend chart (duration, start time, axis preferences, etc.).
View Real-time Updates
When the Trend Card widget is in Live mode, the legend continuously updates to show the current value and the Engineering Units (EGU).
Example: Consider a trend chart monitoring the temperature of a machine:
- When you are in Live mode, the legend displays the current temperature value (75°C) and its engineering units (°C).
- As the machine's temperature changes and new data is received (the temperature rises to 76°C), the legend will automatically update to show 76°C.
Pause the Data Flow
In Live mode, you can pause real-time updates on the trend chart. This option is useful when you want to analyze a specific period without new data appearing on the chart.
- On the toolbar, select
to stop data updates.
- Select
to resume data updates.
Reset the Trend Chart
On the toolbar, select , then
select
to reset the chart.
This will return the chart to its state before any modifications were made after plotting the data.