Trend Run-Time Configuration

Once the chart is live, the runtime customization settings allows for more flexibility and user control when viewing real-time or historical data.

At runtime, select on the chart's toolbar to access the custom settings as shown in the following figure.

Field Name Description
Mode This setting allows you to choose whether you want to view real-time data (Live) or past data (Historical) in the trend chart.
  • Live: Plots real-time data from a Historian server and/or OPC UA server. The data is displayed as it is being collected, which is ideal for monitoring ongoing processes.
  • Historical: Plots historical data from a Historian server. You can review and analyze data that has already been recorded over a specific period.
Note:
Changes made to 'Live' affect 'Historical' as well. For example, if you add/delete properties from the chart in the Live mode, these changes reflect when you shift to the Historical mode as well.
Duration This setting allows you to select the time range of the data you want to view in the chart. You can use the pre-defined intervals (e.g., 1 Minute, 5 Minutes, 1 Hour, etc.) for quick selections. If none of the pre-defined options fit, you can enter your own specific time range by filling out the Custom fields.
Select a duration for which you want to plot the data. The selected duration is subtracted from the End time to deliver past trends. You can go back in time in minutes, hours, days, or provide a customized duration.
  • 1, 5, or 30 minutes
  • 1, 2, 4, 8, or 24 hours
  • 1 week
  • 30 days
  • Choose Custom and enter a different duration in the time format text box.
End Allows to set an end date and time for trending historical data.

Select to update a specific date and time.

  • If you have set a date and time in the past, select Done to apply.
  • If you want to set the current date and time, select Now to apply. The current time can also be set by enabling the toggle switch.
Now Allows to update the End time to your current system time. The toggle is enabled by default when you enter the Historical mode for the first time. Choosing a different date and time automatically disables the toggle.
  • Select to refresh ‘Now’ configured charts. Use this option to instantly update the end time to current time if the chart is already configured for ‘Now’.
  • You can also save a 'Now' configured chart as your favorite. When you reload such charts from favorites, the end time is set to the current system time, and trends are displayed.
    Note:
    After upgrading to 2.1, values from previously saved favorites are updated to represent the range for end time instead of the start time. The ‘Now’ toggle remains disabled for old favorites.
Sampling Increment Select whether you want to increment the sampling data based on time or count, and then specify the time or count, respectively.

Note:
The sampling increment may not always be honored. The maximum number of data points plotted on the trend chart is 3000 when sampling by time, and 8000 when sampling by count. You can zoom in to view more accurate data.
Display You have the option to set a display style on how tags appear across the trend card. The selected display style applies to configured source tags (except third party OPC UA and asset model tags), chart tooltip/legend, and Historian statistical data. Choose from these options:
  • Tag Name: Displays only tag name.
  • Tag Description: Displays only tag description. Lengthy descriptions are truncated with an ellipsis. Move your cursor over ... to reveal the complete description. In the absence of a description, tag name is displayed by default.
  • Tag Name and Description: Displays both tag name and description.
Notes You can add notes only to historical trends, and not for OPC UA based trends.

Switch the toggle to enable viewing or adding a note on the trend chart.

On the trend chart:
  • To add a note for the first time for a specific data point, select the data point, and then select .
  • To access a note, select .
    Note:
    You cannot modify or delete a note; if you want to augment a note, you can add additional notes.
  • To add an additional note for a data point, select .
  • To navigate through multiple notes, use and .

When you access an existing note, the timestamp and tag values that appear during the initial loading of the note correspond to the x-axis and y-axis values for the data point, respectively. If you select each individual note, the actual raw and timestamp values to which the comment was added in the Historian archive appear.

If you add a note to an interpolated value, it is added to the nearest raw value. Due to this, the value displayed in the note may not always match the value plotted on the chart.

Query Criteria Applies to Historical mode, and for Historian data sources only. This option allows you to query tag data based on timestamps.
Note:
Trend via Tag Query can be performed on the tags of the same Historian server only, and not from multiple Historian sources.
If you want to change to a different Historian data source to query tags, do the following:
  1. Clear the check box for all the tags from the current data source and select Apply.
  2. Reopen Tag Query Criteria.
  3. Select the (different) data source tags to add query condition/s.
For example, consider you have two tags in your system - Tag1, Tag2. You can configure a query criteria wherein you request to plot the Tag1 data for last one hour that matches with the conditions applied to the Tag2 data.
  1. Select a duration to plot the data. For example, select 1H.
  2. Select Add Tag Query Criteria to access the Tag Query Criteria screen.

  3. Select a tag from the Proficy Historian data source. The selected tag appears under ADD CONDITIONS.
  4. Expand the tag and set up a condition. You can set up multiple conditions using AND, OR operators.

    For example, you can query Tag1 (multiple tags can be trended) data for the timestamps wherein Tag2 is greater than 100 AND Tag3 is less than 500 OR Tag4 is equal to 300 in the specified time range.

  5. Select Apply.

    The query fetches only the timestamp values where the condition/s are met. Any data that does not match the query criteria is filtered out from the trend chart display. As a result, you may find interrupted trend lines in the chart.

To modify or update any added query conditions, select the pencil icon.

Sources Data can be plotted to the trend chart using properties from an asset model. In the absence of an asset model, you can also directly browse the data source address space and select tags for the trend chart.

Select Add Tags for Trend to select the properties or tags that you want to add to the trend chart.



Tags marked as are from the Historian data source. Tags marked as are from the real time data sources such as iFIX, CIMPLICITY, and any other OPC UA server.

Note:
Nodes only work for plotting historical data. They do not work in Live mode.
SAMPLING MODE For each tag SOURCE, you can add multiple sampling modes. This option is available only for the historical mode.

Select [Add Sampling Mode] to add additional sampling modes for a tag. For example, you can have 3 different sampling modes for a single tag in the trend chart. Highlight each mode with a different line color, style, and thickness.



These are the modes available to plot data:

  • Trend To Raw
  • Minimum
  • Maximum
  • Average
  • Total
  • Standard Deviation
  • Interpolated
  • Lab
  • Lab To Raw
  • Delta
  • Delta Positive
  • Delta Negative

You can trend each tag-sampling mode combination only once. For example, if Trend To Raw mode is applied to Water Temp tag, this mode becomes inactive for this tag. The other modes are available to use.

To delete a plotted sampling mode, select next to the tag.

For more information on the sampling modes, refer to the Historian documentation.

Specification Limits To monitor a process performance, you can define upper, lower, or targeted limits (from varied data sources) and plot these lines on the trend chart.
Provide specification limits for UPPER LIMIT, TARGET, LOWER LIMIT as follows:
  • Enter values manually, (OR)
  • Select Browse to browse the data source and select a tag to populate real-time data (current value).

To highlight each plotted line with a unique line color, thickness, and/or style, choose a COLOR, LINE WEIGHT, and LINE STYLE.



To remove a plotted limit from the chart, select next to the specification limit. You can set the specification limits for both live and historical mode, and save the chart to favorites.

Chart Y Axis Configuration Allows to compare two or more tags/sources by having a common Y-axis on the trend chart. This option is disabled if you selected the Stacked Y-axis mode.

See Customize Y-Axis Display Settings.