Mark a View as a Favorite

A favorite allows you to save a configured view for quick access later.

Favorites can be saved in two distinct ways, each serving a different purpose. Understanding the difference ensures the correct data is loaded when the favorite is used:
  • Context-sensitive: These favorites apply to similar assets, and adapt to any asset with matching properties. When you save a favorite while navigating through an asset (for example, using the Breadcrumb widget), it becomes context-sensitive. This means the favorite can later be applied to any asset that shares the same properties, showing corresponding data for that asset.

    For example, if you save a favorite while viewing Pump1 and include properties like Temperature and RPM, that favorite can later be applied to Pump2, Pump3, or any other asset with those properties.

  • Explicit: These favorites are tied to a specific asset, ensuring that the configuration always loads data from that asset alone.

    From the previous example, to create an explicit favorite linked to Pump1, simply avoid using the Breadcrumb navigation. Instead, configure the favorite specifically for Pump1 properties, ensuring that the saved data is always tied to Pump1.

Creating a Favorite

To save a view as a favorite:
  1. Generate a trend chart.
  2. On the toolbar, select

  3. Enter a name for the favorite.
    Important:
    Do not use special characters like ? / \ # ; % in the name.
  4. Select Add.

Loading a Favorite

To open a saved favorite:
  1. If the favorite is context-sensitive, ensure you have navigated to a valid asset.
    Note:
    If no valid asset is selected when loading a favorite, a warning may appear.
  2. Select the saved favorite from the drop-down list box next to

  3. The system loads the favorite.

Additionally, you can access your saved favorites when creating application pages in Operation Hub. In the Trend Card widget properties, select a favorite view from the Select Favorite drop-down. The selected view will load by default when you launch the chart at runtime.