About Route Type Constraints

The system displays Route Types based on the enabling or disabling of ECO Site parameter in Plant Applications Administrator. Route Types include both standard route types and route types created manually. Standard route types refer to the route types created by the system.

The following section describes the conditions based on which the Route Types and Materials are displayed in the system.

When the ECO Site parameter is: The system displays:
Enabled
  • Route Types: Non-ECO Controlled and From Material
  • Material: Non-ECO Controlled
Disabled All Route Types and Materials
When the ECO Site paramter is: And you select this Route Type: Then the system displays this Material:
Enabled Non-ECO Controlled
  • ECO Controlled
  • Non-ECO Controlled
From Material Non-ECO Controlled
Disabled ECO Controlled
  • ECO Controlled
  • Non-ECO Controlled
Non-ECO Controlled
  • ECO Controlled
  • Non-ECO Controlled
From Material
  • ECO Controlled
  • Non-ECO Controlled