Provide Values for Properties

About this task

When properties are defined in Plant Applications, default value for each property may be provided. Using Route Editor, you can provide values for each property (and overwrite default values if they exist).

Before you begin

Assign a property group to the route or operation.

Procedure

  1. In the Route Editor page, select the route for which you want to provide values for properties.
  2. Select Properties.
    A list of property groups assigned to the route appears.
    Tip:
    If the property has been assigned to an operation, you can select the operation to access a list of property groups assigned to the operation (instead of accessing property groups assigned to all the operations in the route).
  3. Select corresponding to the property group for which you want to provide values.
    A list of properties in the property group appears. If a default value has been provided for a property in the Property Definition module, it appears in the VALUE column.
  4. Enter or modify the value in the VALUE column for each property for which you want to provide a value. The following conditions apply when you provide a value for a property:
    • If a property has been specified as mandatory in the Property Definition module, you must provide a value for the property.
    • The value must be of the same data type as specified in the DATA TYPE column.
  5. Select Save.

Results

The values for the properties are saved.

What to do next

Release the route.