NAME |
The name for the operation. |
BEHAVIOUR |
Select the behavior of the operation. The following options are available:
- Non Clocking: Select this option if the operation does not require a manual clocking on. If you select this option, you can mark an operation complete even if serials/lots are not clocked on, mandatory BOM items are not consumed, or values for mandatory quality variables are not specified.
- Clocking: Select this option if the operation requires manual clocking on and clocking off. By default, Clocking is selected for an operation.
|
LABOR TYPES |
Select the labor types for the operation. A value is required.Note: If the behavior of the operation is set to Non Clocking, this field is disabled. |
DEFAULT LABOR |
Select the default labor type. A value is required. You can choose from the list of values that you selected in the LABOR TYPES column. When an operator clocks on a serial/lot number using the Work Queue or Unit Operations application, by default, the labor type that you select in this column is selected. The operator can, however, choose a different one from the ones that you selected in the LABOR TYPES column.Note: If the behavior of the operation is set to Non Clocking, this field is disabled. |
OPTIONAL |
Switch the toggle to specify if this operation is optional.Note: If you have set all operations as optional, you must at least complete one optional operation to execute the work order. |
MUTUAL EXCLUSION |
Switch the toggle to make the operation as mutually
exclusive to another operation.Note: You can make an
operation mutually exclusive to another operation that
has the same sequence number (priority). |