Transforming grid planning
The PlanOS software platform offers a holistic approach to planning for your energy system's most pressing challenges. Run multiple planning analyses (Power Flow, Production Cost, Resource Adequacy, and Capacity Expansion) using the same base dataset, all from one software interface. Your dataset will seamlessly flow between native simulation functions in this truly integrated planning experience.
In the 1960s, the tools our Engineers needed to understand and operate complex electric grids didn’t exist. So, they built them.
Early simulations explained issues and directly led to innovations in generator protection.
Using our models, planners proved wind could meet 10% of system capacity without compromising reliability.
We didn’t set out to sell this grid planning software, but as utilities began requesting access to our tools, we responded.
What started in New York now supports planners worldwide as they modernize the grid.
The origin of PlanOS
PlanOS was built out of necessity by power system engineers tackling real-world challenges. In the 1960s, our engineers faced a significant challenge: the grid was becoming increasingly complex, but the tools to understand and operate it didn’t exist. So, we built them.
Early models identified the cause of twisted generators and helped develop solutions to mitigate future issues. Over time, the tools evolved to become more advanced, supporting everything from reliability planning to renewable energy integration. As utilities asked to use them, we shared these resources first through time-share systems and later through local installations. What began in New York has expanded into a trusted platform used by planners worldwide. Today, that legacy lives on in PlanOS: a purpose-built software developed by decades of hands-on experience and real-world planning needs.
PlanOS' functions
The PlanOS platform brings together GE Vernova’s decades of proven planning software tools (Production Cost, formerly MAPS*; Resource Adequacy, formerly MARS*; Power Flow) and newly added Capacity Expansion into one powerful interface. PlanOS utilizes one shared dataset to seamlessly transition between analyses, like production cost, resource adequacy, and power flow, without the need for third-party add-ons.
This coordinated and holistic approach to analyzing a power system helps you break down traditional grid modeling silos and enables Integrated Systems Planning analysis.
Looking for PSLF? Visit our PSLF page.
Resources
Explore a collection of playbooks and whitepapers developed to help planners, engineers, and decision-makers better understand the challenges of a rapidly evolving grid, FERC Order 1920, and how Integrated Systems Planning with PlanOS can help address them.
Why planning silos no longer work
As the grid transforms, isolated decisions create financial and reliability risk. This playbook draws on real-world utility challenges to show how shared data, and integrated workflows help utilities invest with confidence.
The imperative for integrated system planning
The energy grid is changing fast, driven by electrification, AI, and renewables. Discover how ISP helps utilities and operators respond to evolving demands, meet regulatory expectations, and plan for a reliable energy future.
Frequently asked questions
Discover the advantages of Integrated Systems Planning and learn more about PlanOS’ functions and capabilities.
Discover more about PlanOS, how it fits into the planning landscape, and why Integrated Systems Planning matters.
With the growth of inverter-based resources and the increase in variable loads on the grid, it’s critical for system planners to consider more comprehensive planning approaches to help identify and solve issues holistically. Integrated Systems Planning is an approach to energy planning that considers all aspects of an energy system aiming to improve the system for cost-effectiveness, sustainability, and reliability by coordinating them together, rather than planning each element separately. This holistic approach provides an improved understanding of resources and their performance while aiming to ensure cost-effective reliability.
Traditionally, the analyses that feed into system planning, like resource adequacy, cost of production, and power flow, are conducted in silos and often rely on different data models, assumptions, and factors. This traditional siloed approach to system planning may result in inaccurate or disassociated insights.
GridOS enables a unified dataset model for the near or real-time operations of the power grid. PlanOS utilizes your dataset focused on long-term planning analysis.
As GE Vernova continues to provide solutions that help you stay ahead of grid complexity, both in terms of operations and planning, the thoughtful architecture of our solution is meant to provide the fidelity of unified data that is appropriate for the context of analysis you need. Spend your time where it matters, planning the grid of the future—not connecting disparate data sets and building multiple data models.
PlanOS provides the high-fidelity, proven engine capabilities you already trust, but in a unified environment that eliminates manual friction. Imagine removing the time spent reconfiguring data or transferring models between power flow, production cost, and resource adequacy tools. With PlanOS, you analyze the same dataset across multiple views instantly, without the need for manual data translation. It’s the same reliable analysis, just faster, seamless, and significantly more efficient.
PlanOS is not just a new user interface, nor is it a new software program. PlanOS is a platform where your unified dataset model can seamlessly flow between GE Vernova’s native modular applications. It is the foundational architecture to streamline data portability, versioning, and branching at speed. For customers with more than one of GE Vernova’s planning functionalities (Power Flow, Resource Adequacy, Production Cost, and Capacity Expansion), the standardized and enhanced user interface provides a consistent user experience that is modern and intuitive.
PlanOS enables cross functional analysis with the same data set. The PlanOS architecture aims to ensure simulations run faster without altering the model unless you intend to for accurate results.
PlanOS’ native infrastructure emphasizes accelerated planning analysis and model portability, helping to eliminate the need for manual data file conversion or the recreation of model format files for analysis.
Explore how PlanOS handles data, tracks assumptions, and connects models so planners can move across studies without losing accuracy or context.
PlanOS was developed with layered data management and version control at its core, so every change in assumptions can be recorded and tracked. When something shifts, such as load forecasts, policy assumptions, or stakeholder inputs, you can create a new branch or version without losing the history. This helps teams stay aligned, since everyone can see what changed, who made the change, and how it affects different scenarios.
PlanOS uses a unified data model built on an entity-model relationship framework, allowing the same input entities and shared transmission parameters to be used across planning functions.
Capacity expansion shifts the transmission network from nodal to zonal, enabling the model to efficiently handle long-term investment decisions. It adds granularity to the decision space by simulating how the system operates economically and how it can be built out over time, accounting for reliability and policy constraints.
When you need more detailed downstream analysis, those zonal results must be translated back to the higher-dimensional nodal network. The team is working with users to address the challenges of nodal site selection.
Yes. Production Cost modeling increases temporal granularity to reflect operational constraints of system resources while simplifying physical Power Flow calculations. As grid complexity grows, it is important to consider operating conditions beyond traditional dispatch used in Power Flow analysis. PlanOS’ data framework was developed to map Production Cost results directly into Power Flow inputs, helping to improve fidelity and accuracy when carrying dispatch conditions into steady-state or dynamic studies.
When processing multiple-generation dispatches or transmission configurations, start by creating a single base case, either a revised network or a branch of the network you’re working with. Set each test as a scenario under that base, so everything stays anchored to the same starting point. Then use the Power Flow and Production Cost tools to study contingencies, re-dispatch, and how flows shift across scenarios.
PlanOS runs as a high-performance compute platform on the server side, whether hosted on-prem or in the cloud. It supports parallel simulations, so larger and more detailed models run faster. Production Cost, Capacity Expansion, Resource Adequacy, and contingency and transfer analysis are all natively parallel. PlanOS can distribute jobs across as many compute resources as you allocate, as long as the server has capacity.
Power Flow runs asynchronously, which means multiple users can submit simulations at the same time, and the system will process them as resources open up.
Learn more about PlanOS’ current capabilities, how well it works with other tools and global requirements, and where the platform is headed as new technologies and customer needs shape future releases.
GE Vernova’s proprietary Contingency Analysis (evaluates the impact of potential issues or unexpected events) and Transfer Analysis (evaluates the maximum amount of power that can be moved without violating system limits) capabilities will be native functionalities available for both Power Flow and Resource Adequacy analysis. This simplifies the number of software applications and APIs needed to interface with the software. Unlike other solutions, GE Vernova’s PlanOS also has built-in algorithmic processing and analytical capabilities. This enables faster analysis without relying on third-party algorithmic processing software, simplifying your IT infrastructure for planning analysis, and helps save your business time and money.
PlanOS is enabled with proprietary APIs for file conversion before or after analysis efforts, making it compatible with most industry file formats and planning software.
Yes, the functions of PlanOS can comply with different grid codes, connection standards, industry mechanisms, and user requirements. This global approach allows GE Vernova to effectively apply lessons learned from developed regions to developing areas, addressing universal and localized grid challenges.
Yes, AI and machine learning (ML) are on the roadmap. The team is exploring collaborations in the AI and ML space, including GenAI and agent-based approaches, and will share more as those capabilities take shape.
GE Vernova collaborates with our customers, system operators, regulators, policymakers, and developers worldwide to incorporate various regulatory and industry-leading enhancements into the software.
Additionally, we are our own customer. GE Vernova’s Consulting Services uses PlanOS for our global studies and assessments. We have developed and maintained commercially available models of over 50 countries, adapting to different grid codes, connection standards, and industry mechanisms.
Still have questions? No worries – we're here to help and will get back to you soon! Contact Us
Resources
Contact us
*Trademark of GE Vernova and/or its affiliates.
**Decarbonization, as used in this document, is intended to mean the reduction of carbon emissions on a kilogram per megawatt hour.