In 2016, electricity consumption in Turkey increased by 4.44% while its electricity generation increased just 4.2%. The country needed to quickly find a way to increase power capacity, reliability, and efficiency while also decreasing emissions. Yeniköy has two units with a total of 420 MW output, while Kemerköy has three units with a total of 630 MW output. Both lignite-fired coal power plants serve around 521,000 homes and meet approximately 5% of Turkey’s energy demands.
GE’s Steam Power business proposed an integrated solution to modernize both plants. The modernization and full plant refurbishment will include replacing five Zamech high-pressure, intermediate-pressure, and low-pressure steam turbines, and five Dolmel generators with air-cooled generators. GE will also upgrade five Rafako boilers, modernize five flue-gas desulfurization and electrostatic precipitator systems, as well as the electrical and mechanical balance of plant, and will install a distributed control system.
increased efficiency
Decreasing NOx emissions to new level
increase in both plants’ capacity
GE has a strong local presence and offers us a one-stop-shop service provider for all of our modernization needs. With these upgrades, our plants will be better-positioned to meet the future energy needs of Turkey's residents and businesses.
Serhat Ceçen
Chairman, IC IÇTAŞ Enerji Investment Holding and Yeniköy Kemerköy Elektrik Üretim Ve Ticaret A.Ş.
The upgrade of the two facilities will help increase the plants’ capacity by 197.5 MW—enough to additionally power the equivalent of approximately 198,000 homes—while also significantly decreasing plant emissions. The plants’ efficiency will improve by 6 percentage points, to 40%.
The project, with Yeniköy Kemerköy Elektrik Üretim ve Ticaret A.Ş. is the latest example of GE’s commitment to modernizing coal-fired power plants and generation equipment around the globe.
The upgrade solutions will extend the lifetime of the power equipment by 20 years and significantly lower emissions at the two power plants to meet country’s emission limits, including:
By bringing together cross-business expertise and technologies, GE’s Powering Efficiency COE can apply a total-plant hardware and software solution approach, in turn boosting the efficiency of the world’s new and existing coal-fired power plants and significantly reducing their emissions.