Back-end burnout: How 7Extend and the upgraded radial diffuser can help relieve exhaust system stress
Jay Bryant
September 26, 2025
1 min read
As 7E units age, the back end takes a hit—from cracking to seal failures and mounting backpressure. With 7Extend and the upcoming advanced radial diffuser, operators have new options to help bring life and output back into balance.
The exhaust section of the 7E turbine is no stranger to fatigue. Over time, common issues include:
These issues chip away at performance—and drive up both costs and outage hours.
The 7Extend package already includes upgraded exhaust components, including:
Looking to go further? The advanced radial diffuser, coming in 2026, introduces a reimagined flow path:
Built on a proven 9E.04 concept, this update helps bring up to 1 MW of output recovery and up to ~0.5% heat rate improvement—all while helping to reduce future repair needs.
Exhaust fatigue doesn’t need to be a recurring issue. With 7Extend—and a look toward radial diffuser tech—7E operators can take real steps toward restoring performance and cutting unplanned O&M. Together, these updates help position your unit for what’s ahead—without the wait or cost of building new.

7E Product Manager, GE Vernova
Jay has served as the product manager for the 7E family of gas turbines for 9 years, overseeing over 1,100 units in 27 countries. During his 26+ years at GE Vernova, his experience includes global supply chain, quality, and commercial intelligence, notably as the commercial director for B/E multi-year service agreements. Jay holds degrees in Electrical Engineering from the University of Kentucky and an M.B.A. from the University of South Carolina.
Contact us
*Trademark of GE Vernova and/or its affiliates.