Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / EnumeratedSetChangedEvent Event


EnumeratedSetChangedEvent Event (ServerConnection)
Occurs in response to enumerated set subscriptions when a set has been added, deleted, modified or renamed.
Syntax
Public Event EnumeratedSetChangedEvent As EnumeratedSetChangedHandler
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also